FB#.P

Description

This parameter reads the raw position of the corresponding feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position. The position is given in counts. The output format is 32:32, the upper 32 bits represent the multi-turns and the lower 32 bits represent the position of the feedback.

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Counts

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.